This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VPIF - Memory connection

Other Parts Discussed in Thread: OMAP-L138

Hello,

I am having difficulties in understanding the connection between the VPIF peripheral and the memory (any available) in the OMAP-L138 processor.

More particularly,I have two questions (maybe too naive!):

1) I am not sure if the VPIF  peripheral is directly connected to memory through a DMA interface as depicted in page 1743 of OMAP-L138 TRM.
In other words, if I have allocated in DDR2 two buffers in which I store the incoming frames from the VPIF peripheral.These buffers are filled without the intervention of the ARM/DSP ?

2) Is the EDMA controller used by the VPIF peripheral,or it is just a DMA controller available to the programmer and it is not used by any peripheral that claims to have DMA access.

Thank you in advance!