The AM335x TRM is confusing. The TRM seems to indicate there is two dedicated DMA channels as part of the SD/MMC/SDIO IP block. But then again it states that DMA master mode is not supported.
My question is are the SD/MMC IPs block DMAs functional or do you have to use the EDMA controller and two channels from it?