Hi TI experts
I am using ipnc rdk v3.5, when I am testing stability of my application, I am getting this issue frequently.
[m3video] ENCLINK:H264Enc !!WARNING!!!Unable to handle runtime output buffer request
[m3video] Extended error 18400 for reqObjIndex 0
[m3video] Extended error 18000 for reqObjIndex 1
[host] Error code: -1 at 468
[host] Error code: -1 at 468
[host] Error code: -1 at 468
[m3video] 276397:WARN
[m3video] ENCLINK:ERROR in Enclink_h264EncodeFrameBatch.Status[-1] for IVAHD_0
[m3video] 276397:WARN
[m3video] ENC : IVAHDID : 0 ENCLINK:ERROR in EncLink_SubmitBatch.Status[-1]
[m3video] Extended error 18000 for reqObjIndex 0
[m3video] 276399:WARN
[m3video] ENCLINK:ERROR in Enclink_h264EncodeFrameBatch.Status[-1] for IVAHD_0
[m3video] 276399:WARN
[m3video] ENC : IVAHDID : 0 ENCLINK:ERROR in EncLink_SubmitBatch.Status[-1]
[m3video] Extended error 18000 for reqObjIndex 0
[m3video] Unhandled Exception:
[m3video] Exception occurred in ThreadType_Task
[m3video] handle: 0x953811e4.
[m3video] stack base: 0x954f7900.
[m3video] stack size: 0x2000.
[m3video] R0 = 0x9b260000 R8 = 0x00000780
[m3video] R1 = 0x13493c30 R9 = 0x00000438
[m3video] R2 = 0x09d10510 R10 = 0x954fabd8
[m3video] R3 = 0x00000000 R11 = 0x00000000
[m3video] R4 = 0x954f9900 R12 = 0x9b260000
[m3video] R5 = 0x954fac40 SP(R13) = 0x954f97e8
[m3video] R6 = 0x906b31c4 LR(R14) = 0x94d61d33
[m3video] R7 = 0x00000000 PC(R15) = 0x94d6b658
[m3video] PSR = 0x21000200
[m3video] ICSR = 0x0440f803
[m3video] MMFSR = 0x00
[m3video] BFSR = 0x82
[m3video] UFSR = 0x0000
[m3video] HFSR = 0x40000000
[m3video] DFSR = 0x00000000
[m3video] MMAR = 0x13493c30
[m3video] BFAR = 0x13493c30
[m3video] AFSR = 0x00000000
[m3video] Terminating Execution...
I am not able to run my usecase application for more than an hour ( 1 h maximum).
Can someone help me to resolve this issue.
I have already changed this macro:
#define UTILS_ENCDEC_GET_BITBUF_SIZE(width,height,bitrate,framerate) \ (((width) * (height) )