Other Parts Discussed in Thread: OMAP-L138, DA8XX
Hi everyone,
I got the ZOOM OMAP-L138 EVM DEVELOPMENT KIT and DaVinci-PSP-SDK-03.20.00.06 with Arago distribution developed by TI for OMAP processor.
I'm currently trying to boot from the parallel NOR flash. I compiled a kernel and build a filesystem for the NOR flash. I flashed into the NOR the original UBL given with the SDK and my own u-boot compiled with the define to boot from the NOR. The board is booting without any problem.
Now, I would like to boot in less than 5 seconds (I did it in 10 seconds with nfs). On boot, to reduce the data to transfer from the NOR flash to the RAM, I configured the filesystem to be permanent in the NOR flash. Otherwise, I applied most of trick in this wiki:http://wiki.davincidsp.com/index.php?title=All_This_For_1_Second_Boot
There is one thing I'm not able to do from the wiki. I would like to increase the speed of the NOR flash. It's currently very slow, I tried to change the NOR EMIFA CS2 settings but it's not working. In fact, I'm not able to find the file ../u-boot/board/davinci/lowlevel_init.S". The only thing that looks like that is under "../u-boot/cpu/arm926ejs/davinci/lowlevel_init.S" or "../u-boot/cpu/arm926ejs/da8xx/lowlevel_init.S".
I tried to modify both files with the assembly code proposed and no change when reading the kernel from the NOR flash.
--
ACFG2: .word 0x01E00010
ACFG2_VAL: .word 0x3FFE058D
LDR R0, ACFG2
LDR R1, ACFG2_VAL
LDR R2, [R0]
AND R1, R2, R1
STR R1, [R0]
--
In an other hand, I tried to build my own UBL with "AISgen for D800K002" and I set the CS2 Setup in Flash tab with 0x3FFE058D. Same thing the transfer is still very slow.
I searched on many website to find the answer, the solution was always to modify "../u-boot/board/davinci/lowlevel_init.S".
Anyone know how to solve this issue?
Thank you for the support.
Nicolas