Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hello,
I have an OMAP-L138 LCDK and an XDS100v2 JTAG Emulator. I am attempting get "any" of the StarterWare for OMAP-L138 to run for ARM. I have gotten DSP side examples to run. I am using CCSv5. I am using the OMAPL138_ARM.gel that can be found in the StarterWare directory. I have all LCDK DIP switches set to off. When I attempt debug spi_edma_arm5_omapl138_lcdkOMAPL138 I get the following error (below). I have tried other Arm projects and get the same problem. I am not sure why. I could send a cleaned zip of my project (since its just the StarterWare w/ directories changed) to anyone that thinks they could help me solve this. Thanks, Phil
ARM9_0: Output: Target Connected.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Cleared.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Setup Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: KICK Unlocked.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: PSC Enable Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: GEL: Error while executing OnTargetConnect(): Target failed to write 0x01C11138 at (*((unsigned int *) (0x01C11000+0x138))|=0x1) [OMAPL138_ARM.gel:16] at device_PLL0(0, 24, 1, 0, 1, 11, 5) [OMAPL138_ARM.gel:400] at Set_Core_300MHz() [OMAPL138_ARM.gel:459] at Core_300MHz_mDDR_150MHz() [OMAPL138_ARM.gel:247] at OnTargetConnect() .