This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 EVM or C5505 EVM

Hi

I want to buy an evaluation module for active noise(vibration) control. In this applcation I have some piezoelectrics as sensors and actuators. I get the data of sensors through stereo codec inputs, do processing on them then send data to actuators through stereo codec outputs. I want to know that which of C5515 EVM or C5505 EVM is suitable and cost effective for my application. (The input and output of piezoelectrics are compatible with sound card of PC soI guess that it also will be compatible with stereo codec)

Thanks