This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tcp3e

welcome  ,

iam new in multicore dsp  iam working in tcp3e module i read the pdf and open the example code in code composer 

my question: is this example is the simplified one or i could write some code that is more simplified  to runthe module and had the minmum options in the tcp3e or is there already a simplified one 

please advice me with material and ideas to help me to write  such simple code to just run the tcp3e moddule in multicore c6670

thanks in advance 

  • Hi,

    Unfortunately that is the only example we provide as part of MCSDK.

    Since you are using C6670, did you look at BCP User Guide for Turbo Encoding? There is a turbo encoder sub-module in it which is much easier to program and it is packet DMA based rather than EDMA based. 

    Regards,

    Arun