This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x Android boot problem PVR_K: User requested SGX debug info

Dear All,

I'm trying to boot Android on DM814x, I'm new on this platform and I don't understand the error reported. I attached boot log file. I will appreciate your commentaries.

HDMI W1 rev 4.0
ti81xxfb ti81xxfb: failed to stop.
warning: `zygote' uses 32-bit capabilities (legacy support in use)
alarm_set_rtc: no RTC, time will be lost on reboot
detected fb_set_par error, error code: -110
omaplfb: OMAPLFBFlip: Device 0: fb_set_var failed (Y Offset: 1080, Error: -110)
PVR_K: User requested SGX debug info
PVR_K: SGX debug (1.7.17.4352)
PVR_K: Flip Command Complete Data 0 for display device 1:
PVR_K: SRC 0: ROC DevVAddr:0xD80006C ROP:0x2 ROC:0x0, WOC DevVAddr:0xD800064 WOP:0x1 WOC:0x0

Thanks in advanced, kind regards

Alejandro