Hi
The GLSDK now I use is 6_03_00_01, now I finish the setup of the GLSDK ,how to link the ubuntu host with the omap5432 on NFS, so I can compile the program easier
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The GLSDK now I use is 6_03_00_01, now I finish the setup of the GLSDK ,how to link the ubuntu host with the omap5432 on NFS, so I can compile the program easier
thanks
Hi Michael,
if you run the GLSDK 6.03.x setup script setup.sh in the GLSDK folder, you will be asked whether you want to use SD card or NFS root filesystem. I suggest checking that option for getting the NFS root filesystem from your Ubuntu host mounted on the EVM.
Regards,
Marc