Hi TI Experts,
( The below errors are already posted by Rajesh Singh on 28Feb14, can you reply your solutions or suggestions based on this issue quickly, so that we can overcome this issue because we are struggling with this issue for long time )
I am using ipnc rdk v3.5, when I am testing stability of my application, I am getting this issue frequently.
[m3video] ENCLINK:H264Enc !!WARNING!!!Unable to handle runtime output buffer request
[m3video] Extended error 18400 for reqObjIndex 0
[m3video] Extended error 18000 for reqObjIndex 1
[host] Error code: -1 at 468
[host] Error code: -1 at 468
[host] Error code: -1 at 468
[m3video] 276397:WARN
[m3video] ENCLINK:ERROR in Enclink_h264EncodeFrameBatch.Status[-1] for IVAHD_0
[m3video] 276397:WARN
[m3video] ENC : IVAHDID : 0 ENCLINK:ERROR in EncLink_SubmitBatch.Status[-1]
[m3video] Extended error 18000 for reqObjIndex 0
[m3video] 276399:WARN
[m3video] ENCLINK:ERROR in Enclink_h264EncodeFrameBatch.Status[-1] for IVAHD_0
[m3video] 276399:WARN
[m3video] ENC : IVAHDID : 0 ENCLINK:ERROR in EncLink_SubmitBatch.Status[-1]
[m3video] Extended error 18000 for reqObjIndex 0
[m3video] Unhandled Exception:
[m3video] Exception occurred in ThreadType_Task
[m3video] handle: 0x953811e4.
[m3video] stack base: 0x954f7900.
[m3video] stack size: 0x2000.
[m3video] R0 = 0x9b260000 R8 = 0x00000780
[m3video] R1 = 0x13493c30 R9 = 0x00000438
[m3video] R2 = 0x09d10510 R10 = 0x954fabd8
[m3video] R3 = 0x00000000 R11 = 0x00000000
[m3video] R4 = 0x954f9900 R12 = 0x9b260000
[m3video] R5 = 0x954fac40 SP(R13) = 0x954f97e8
[m3video] R6 = 0x906b31c4 LR(R14) = 0x94d61d33
[m3video] R7 = 0x00000000 PC(R15) = 0x94d6b658
[m3video] PSR = 0x21000200
[m3video] ICSR = 0x0440f803
[m3video] MMFSR = 0x00
[m3video] BFSR = 0x82
[m3video] UFSR = 0x0000
[m3video] HFSR = 0x40000000
[m3video] DFSR = 0x00000000
[m3video] MMAR = 0x13493c30
[m3video] BFAR = 0x13493c30
[m3video] AFSR = 0x00000000
[m3video] Terminating Execution...
I am not able to run my usecase application for more than an hour ( 1 h maximum).
Can someone help me to resolve this issue.
I have already changed this macro:
#define UTILS_ENCDEC_GET_BITBUF_SIZE(width,height,bitrate,framerate) \ (((width) * (height) )