This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[SOLVED] Connection failed "Device_Name" after opening any Remote Tool..

Hello Friends,

 I am trying to use Remote Tools for Registry checking. My build option properties are as :

Enable KITL Yes

Enable Profiling= Yes

and I have build the image in release build. 

And in connectivity option, I have selected Add Device with Name TEST_MY_DEVICE

and remaining options are default options.. when i image downloaded successful on the Target device via Ethernet my console display message as

Connecting to Desktop
KITL: Connected host  IP: 192.168.1.26  Port: 64429
KITL connected with Desktop

Then i click on Remote tools and select Registry Editor then i select my device name under Platform Builder as TEST_MY_DEVICE and click on okay.. It try to establishing a connection between host and target device but at the end I always got a message as connection failed ........

Any one can help me regarding this issue ???