Hi TI Tech support,
I have to port ad9361 driver to 3.2.0 linux kernel,but the ad9361 driver is compatible with 3.12.x kernel
because path of the driver location is different.
and also device is connected through SPI interface with AM335x processor EVM board.
Please guide me how to port the driver from latest kernel to 3.2.0 kernel.
Thanks
Murugan