Other Parts Discussed in Thread: MSP430F5338, MSP430F5529
Hi,
1. We are using MSP430F5338, TI-RTOS 1.20.00.28, CCS 5.5.0.00077
2. SD card : SnaDisk 8GB, SDHC, class-4 formatted FAT32 on Windows 7 system.
Issues :
1. Card recognizes as SDSC instead of SDHC.
2. I made few changes in fatsf dir but I can not build bios. The log file attached.
command : C:\ti\tirtos_1_20_00_28>..\xdctools_3_25_04_88\gmake.exe -f tirtos.mak bios
Errors : Starting build of library sources ...
Build of libraries failed.
error: xdc.cfg.SourceDir: "C:/ti/xdctools_3_25_04_88/packages/xdc/cfg/SourceDir.
xs", line 184: xdc.cfg.SourceDir : Build of generated source libraries failed: e
xit status = 2:
cmd.exe: not found
Clarification :
1. Do TI-RTOS and fatfs provided by TI support 8/16/32 GB SDHC cards ?
2. Is there any restrictions on make, size and class of SD card ?
Thanks