This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

demo don't work with Beaglebone Black

Hello

the demo app don't work with the Beaglebone Black.

I use Starterware 2.0.1.1 with the patch for Beaglebone Black

The console give the following output

StarterWare AM335x Boot Loader

Copying application image from MMC/SD card do RAM

Jumping to StarterWare Application

Board Name: A335BNL

Board Version: 0A5C

SoC Version: 1

CM3 Firmware Version 358

 

I guess it stucks at the init of the timer

Has anyone a working app for the Beaglebone Black with timer1 init?

regards Tobias