Other Parts Discussed in Thread: MATHLIB
I am having an issue with linking to these libraries.
In the code I put:
#include <include>
In project I have added the following include paths:
C:/Program Files (x86)/Texas Instruments/mathlib_c674x_3_0_1_1/inc
and
C:/Program Files (x86)/Texas Instruments/mathlib_c674x_3_0_1_1/packages
When I select open declaration inside the main code I get the header file with the includes in the src directory so the include paths seems to be working. But when I select open declaration (cossp for example) I get nothing. With I try to compile I get the famous "unresolved symbol cossp, first referenced in ./main.obj" error message.
The same thing happens when I try using the dsplib. Any suggestions?