Hi,
I am testing the MAD Utility using C6678 EVM.
I use the document below:
http://processors.wiki.ti.com/index.php/MAD_Utils_User_Guide
According to the steps in the Demo walkthrough, use the build_examples_msys.sh, I can the build the example code.
But in my project, the SYSBIOS is used, so I must build my project with CCS IDE(CCS5.2).
My question is, when I build my project, If I want to use the Prelinker bypass mode, what should be set in the CCS5.2.1?And If I want to use the Prelinker mode, what should be set ?
Should the library used in the project (edma, platform_lib...etc) be rebuilt too?
Regards,
Yin