Hi there, I'm trying to get valgrind to build on the tci6638 using bitbake and yocto. I get the following error.
ERROR: valgrind was skipped: incompatible with host arm-oe-linux-gnueabi (not in COMPATIBLE_HOST)
NOTE: Runtime target 'valgrind' is unbuildable, removing...
In valgrind_3.7.0.bb we have the following two lines
COMPATIBLE_HOST = '(i.86|x86_64|powerpc|powerpc64).*-linux'
COMPATIBLE_HOST_armv7a = 'arm.*-linux'
I see this is some kind of override.. in the bitbake manual
So I assume i need to add a line like
OVERRIDES += ":armv7a"
but my question is where do I add this line? Everywhere I've tried so far does not seem to trigger the override.
Can anyone tell me where I'm going wrong?
Cheers
Ville