Hi all,
I am using XTCIEVMK2X EVM.
Developing environment is: CCS ver 5.4.0.00091; MCSDK Packages: 3_00_01_12
Bootmode: ARM SPI Little Endian mode.
I have observed the below errors thrown by ARM while executing our application code on DSP.
run succeded
root@172:~# [ 51.359889] ------------[ cut here ]------------
[ 51.364514] WARNING: at drivers/hwqueue/keystone_hwqueue.c:349 khwq_unmap+0xd0/0x104()
[ 51.372404] Modules linked in:
[ 51.375485] [<c00154c8>] (unwind_backtrace+0x0/0xf8) from [<c0020ee8>] (warn_slowpath_common+0x4c/0x64)
[ 51.384861] [<c0020ee8>] (warn_slowpath_common+0x4c/0x64) from [<c0020f1c>] (warn_slowpath_null+0x1c/0x24)
[ 51.394497] [<c0020f1c>] (warn_slowpath_null+0x1c/0x24) from [<c02fff0c>] (khwq_unmap+0xd0/0x104)
[ 51.403353] [<c02fff0c>] (khwq_unmap+0xd0/0x104) from [<c02215a8>] (chan_complete+0xec/0x6a0)
[ 51.411860] [<c02215a8>] (chan_complete+0xec/0x6a0) from [<c02221b0>] (chan_control+0x218/0xb1c)
[ 51.420629] [<c02221b0>] (chan_control+0x218/0xb1c) from [<c02a1e8c>] (netcp_poll+0x54/0xb4)
[ 51.429052] [<c02a1e8c>] (netcp_poll+0x54/0xb4) from [<c03211ec>] (net_rx_action+0x118/0x26c)
[ 51.437566] [<c03211ec>] (net_rx_action+0x118/0x26c) from [<c0028224>] (do_current_softirqs+0x190/0x324)
[ 51.447028] [<c0028224>] (do_current_softirqs+0x190/0x324) from [<c0028488>] (local_bh_enable+0x60/0x78)
[ 51.456491] [<c0028488>] (local_bh_enable+0x60/0x78) from [<c0071e9c>] (irq_forced_thread_fn+0x40/0x54)
[ 51.465865] [<c0071e9c>] (irq_forced_thread_fn+0x40/0x54) from [<c0071fc0>] (irq_thread+0x110/0x180)
[ 51.474978] [<c0071fc0>] (irq_thread+0x110/0x180) from [<c00410ac>] (kthread+0x9c/0xa4)
[ 51.482964] [<c00410ac>] (kthread+0x9c/0xa4) from [<c000dd18>] (ret_from_fork+0x14/0x3c)
[ 51.491030] ---[ end trace 0000000000000002 ]---
[ 51.495640] dma dma0chan2: failed to unmap descriptor 0x007137c0
root@172:~# [ 52.109746] ------------[ cut here ]------------
[ 52.114361] WARNING: at drivers/hwqueue/keystone_hwqueue.c:349 khwq_unmap+0xd0/0x104()
[ 52.122250] Modules linked in:
[ 52.125318] [<c00154c8>] (unwind_backtrace+0x0/0xf8) from [<c0020ee8>] (warn_slowpath_common+0x4c/0x64)
[ 52.134693] [<c0020ee8>] (warn_slowpath_common+0x4c/0x64) from [<c0020f1c>] (warn_slowpath_null+0x1c/0x24)
[ 52.144324] [<c0020f1c>] (warn_slowpath_null+0x1c/0x24) from [<c02fff0c>] (khwq_unmap+0xd0/0x104)
[ 52.153176] [<c02fff0c>] (khwq_unmap+0xd0/0x104) from [<c02215a8>] (chan_complete+0xec/0x6a0)
[ 52.161681] [<c02215a8>] (chan_complete+0xec/0x6a0) from [<c02221b0>] (chan_control+0x218/0xb1c)
[ 52.170448] [<c02221b0>] (chan_control+0x218/0xb1c) from [<c02a1e8c>] (netcp_poll+0x54/0xb4)
[ 52.178869] [<c02a1e8c>] (netcp_poll+0x54/0xb4) from [<c03211ec>] (net_rx_action+0x118/0x26c)
[ 52.187378] [<c03211ec>] (net_rx_action+0x118/0x26c) from [<c0028224>] (do_current_softirqs+0x190/0x324)
[ 52.196839] [<c0028224>] (do_current_softirqs+0x190/0x324) from [<c0028488>] (local_bh_enable+0x60/0x78)
[ 52.206300] [<c0028488>] (local_bh_enable+0x60/0x78) from [<c0071e9c>] (irq_forced_thread_fn+0x40/0x54)
[ 52.215672] [<c0071e9c>] (irq_forced_thread_fn+0x40/0x54) from [<c0071fc0>] (irq_thread+0x110/0x180)
[ 52.224782] [<c0071fc0>] (irq_thread+0x110/0x180) from [<c00410ac>] (kthread+0x9c/0xa4)
[ 52.232767] [<c00410ac>] (kthread+0x9c/0xa4) from [<c000dd18>] (ret_from_fork+0x14/0x3c)
[ 52.240835] ---[ end trace 0000000000000003 ]---
[ 52.245442] dma dma0chan2: failed to unmap descriptor 0x00000020
Could you please provide the reason for this behavior ? How to avoid it ?
Thanks in advance.
Thanks,
Rajanikanth.