This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building Qt 4.8.5 for dm365

I'm trying to build Qt 4.8.5 for DaVinci DM365.

I copied mkspecs/qws/linux-arm-gnueabi-g++ and named it dm365 so here's how my qmake.conf looks like:

include(../../common/linux.conf)
include(../../common/gcc-base-unix.conf)
include(../../common/g++-unix.conf)
include(../../common/qws.conf)

# modifications to g++.conf
QMAKE_CFLAGS_RELEASE        = -03 -march=armv5te
QMAKE_CXXFLAGS_RELEASE      = -03 -march=armv5te
QMAKE_CC                    = arm-none-linux-gnueabi-gcc
QMAKE_CXX                   = arm-none-linux-gnueabi-g++
QMAKE_LINK                  = arm-none-linux-gnueabi-g++
QMAKE_LINK_SHLIB            = arm-none-linux-gnueabi-g++

# modifications to linux.conf
QMAKE_AR                = arm-none-linux-gnueabi-ar cqs
QMAKE_OBJCOPY           = arm-none-linux-gnueabi-objcopy
QMAKE_STRIP             = arm-none-linux-gnueabi-strip

load(qt_config)

Here's list of options I use for configure script:

./configure -embedded arm -platform qws/linux-x86-g++ -xplatform qws/dm365 -depths 16,24,32 -no-mmx -no-3dnow -no-sse -no-sse2 -no-cups -no-largefile -no-accessibility -no-openssl -no-gtkstyle -qt-mouse-pc -qt-mouse-linuxtp -qt-mouse-linuxinput -plugin-mouse-linuxtp -plugin-mouse-pc -fast -no-qt3support -opensource -no-webkit -no-openssl -nomake demos -nomake examples

After Makefile is created and I try to make to actually build Qt, I get this error:

release-shared/parser.o: In function `Parser::note(char const*)':
parser.cpp:(.text+0x23c): undefined reference to `qt_assert_x(char const*, char const*, char const*, int)'
parser.cpp:(.text+0x276): undefined reference to `qt_assert(char const*, char const*, int)'
release-shared/parser.o: In function `QVector<Symbol>::at(int) const':
parser.cpp:(.text._ZNK7QVectorI6SymbolE2atEi[_ZNK7QVectorI6SymbolE2atEi]+0x2d): undefined reference to `qt_assert_x(char const*, char const*, char const*, int)'
release-shared/parser.o: In function `QStack<QByteArray>::top()':
parser.cpp:(.text._ZN6QStackI10QByteArrayE3topEv[_ZN6QStackI10QByteArrayE3topEv]+0x1f): undefined reference to `qt_assert(char const*, char const*, int)'
collect2: error: ld returned 1 exit status
make[1]: *** [../../../bin/moc] Error 1
make[1]: Leaving directory `/home/dmitry/Downloads/qt-everywhere-opensource-src-4.8.5/src/tools/moc'
make: *** [sub-moc-make_default-ordered] Error 2