This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DM6467T's TSK_sleep

My Linux Kernel is 2.6.32, downloaded from TI's website, it is abnormal when I call TSK_sleep in DSP Side.

At Beginning, It is blocked in DSP Side, not return.

Then, I found the timer's configuration in Linux Kernel as following:

1)enable timer0

2)config T0_BOT as clock event, T0_TOP as clock source,T1_BOT reversed for DSP.

So, I enable the timer1 in the function of davinci_timer_init in arch/arm/mach-davinci/time.c as following:

 timer_clk1 = clk_get(NULL, "timer1") ;
 BUG_ON(IS_ERR(timer_clk1)) ;
 clk_enable(timer_clk1) ;

at the same time, I modified the INPUTCLK in .tcf for DSP Side as following:

prog.module("CLK").INPUTCLK = 247.5 ;

After above two modification, I fount it does not block, it has response !

But, the real time is abnormal, such as:

TSK_sleep(2), the real time is about 2S;

TSK_sleep(20), the real time is about 20S;

I guress the INPUTCLK is not correct, so I modified it to 247500,but the real time is still abnormal:

TSK_sleep(2), the real time is about 1.7S;

I modified it to 247500000,but the real time is still abnormal:

TSK_sleep(2), the real time is about 14ms.

In a word, I guess the INPUTCLK is not correct, but I do not know how to modify it.

So, I want to need some help from TI's experts. Would you tell me how to config the timer0 and timer1 in Linux Kernel and DSP Server ?

Thank you very much