This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 SRIO 1x/2x/4x configuration

Hi TI engineer:

        We have an application to connect C6657 to FPGA in 2 1xport. Now it's not successful,for investigating the problem,can you tell me:

        1.if I config port 0 1 2 3 to path mode0, then I divide SRIO to four 1x port,isn't it? 

         2.If I config port 0 1 to path mode0,then I divide SRIO to two 1x port, and what I do to port 2 3 will be unmeanningful,isn't it?

         3.when srio works in 2 or 4 1xport, each port can connect to target, they don't influence on each other at all, isn't it?

          Look forward to reply, thank you very much!