This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Some questions about C6747's McASP



Hello:

    I configured mcasp0 to TDM mode: I2S mode,slot size is 32 bit,configured srctl0 to receiver and configured srctl6 to transmiter.

   In main function ,if I write data in xbuf6,then rbuf6 changes to the same data.why?

   And there are always 0 in rbuf0, rstat is 0x171.why?

   Rstat is  cleared by writing 1,but in main function it can not be cleard even though I write 1.why?

   In  interrupt  function,can not receive data,initialization and interrupt function are as follows:

Initialization:

mcasp0Regs->GBLCTL=0;
mcasp0Regs->RGBLCTL=0;
mcasp0Regs->XGBLCTL=0;
//mcasp0Regs->PWRDEMU=1;
// mcasp0Regs->DLBCTL=0x07;

mcasp0AfifoRegs->WFIFOCTL = CSL_AFIFO_WFIFOCTL_WENA_DISABLED; //Write FIFO is disabled.
mcasp0AfifoRegs->RFIFOCTL = CSL_AFIFO_RFIFOCTL_RENA_DISABLED;

/*******工作模式配置*****************/
/************RX**********************/
mcasp0Regs->RMASK=0xFFFFFFFF; // All bit enable
mcasp0Regs->RFMT = (0<<16 | 1<<15 | 0xF<<4 | 1<<3 | 0);

//接收帧同步:TDM(I2S) mode;接收帧同步宽度:一个字宽;外部产生;上升沿表示帧的开始。
mcasp0Regs->AFSRCTL = (CSL_MCASP_AFSRCTL_RMOD_I2S << CSL_MCASP_AFSRCTL_RMOD_SHIFT)|\
(CSL_MCASP_AFSRCTL_FRWID_WORD << CSL_MCASP_AFSRCTL_FRWID_SHIFT)|\
(CSL_MCASP_AFSRCTL_FSRM_EXTERNAL << CSL_MCASP_AFSRCTL_FSRM_SHIFT)|\
(CSL_MCASP_AFSRCTL_FSRP_FALLINGEDGE << CSL_MCASP_AFSRCTL_FSRP_SHIFT);

//接收时钟控制:接收器在串行时钟的上升沿采样数据;外部接收时钟源;接收位时钟分频比为:1
/* mcasp0Regs->ACLKRCTL = (CSL_MCASP_ACLKRCTL_CLKRP_FALLINGEDGE << CSL_MCASP_ACLKRCTL_CLKRP_SHIFT)|\
(CSL_MCASP_ACLKRCTL_CLKRM_INTERNAL << CSL_MCASP_ACLKRCTL_CLKRM_SHIFT)|\
(0x03 << CSL_MCASP_ACLKRCTL_CLKRDIV_SHIFT);*/
//接收时钟检查控制寄存器
//mcasp0Regs->RCLKCHK = CSL_MCASP_RCLKCHK_RESETVAL;// RCLKCHK0=0xFF000F; // Doesn't care

//接收高频时钟控制:外部时钟源;接收位流高频时钟极性:上升沿,不翻转;接收高频时钟分配比:1
mcasp0Regs->AHCLKRCTL = (CSL_MCASP_AHCLKRCTL_HCLKRM_EXTERNAL << CSL_MCASP_AHCLKRCTL_HCLKRM_SHIFT)|\
(CSL_MCASP_AHCLKRCTL_HCLKRP_NOTINVERTED << CSL_MCASP_AHCLKRCTL_HCLKRP_SHIFT)|\
(0x00 << CSL_MCASP_AHCLKRCTL_HCLKRDIV_SHIFT);//AHCLKR0=24.576MHz/2=12.288MHz
//接收TDM时隙寄存器:slot0,slot1是活跃的
mcasp0Regs->RTDM = (Uint32) 0x03;


//接收中断控制寄存器:中断全部使能
mcasp0Regs->RINTCTL = 0x00000020;
mcasp0Regs->RCLKCHK = 0x00FF0008;
//EDMA EVENT GENERATE
//mcasp0Regs->XEVTCTL = CSL_MCASP_XEVTCTL_XDATDMA_ENABLE;
/***** TX *****/
mcasp0Regs->XMASK = (Uint32) 0xFFFFFFFF; //发送数据所有位都不屏蔽.
mcasp0Regs->XFMT = (0<<16 | 1<<15 | 0xF<<4 | 1<<3 | 0); //发送位延迟: 0位延迟
//接收串行位流顺序:MSB先发送
//时隙大小为32位
//Reads from XRBUF[n] originate on the DMA port.
//no rotation.
//mcasp0Regs->XEVTCTL = CSL_MCASP_XEVTCTL_XDATDMA_ENABLE;
//发送帧同步:TDM(I2S) mode;发送帧同步宽度:一个字宽;外部产生;上升沿表示帧的开始。
mcasp0Regs->AFSXCTL = (CSL_MCASP_AFSXCTL_XMOD_I2S << CSL_MCASP_AFSXCTL_XMOD_SHIFT)|\
(CSL_MCASP_AFSXCTL_FXWID_WORD << CSL_MCASP_AFSXCTL_FXWID_SHIFT)|\
(CSL_MCASP_AFSXCTL_FSXM_INTERNAL << CSL_MCASP_AFSXCTL_FSXM_SHIFT)|\
(CSL_MCASP_AFSXCTL_FSXP_FALLINGEDGE << CSL_MCASP_AFSXCTL_FSXP_SHIFT);
//发送时钟控制:发送器在串行时钟的上升沿发送数据;发送和接收同步外部接收时钟源;发送位时钟分频比为:4
mcasp0Regs->ACLKXCTL = (CSL_MCASP_ACLKXCTL_CLKXP_FALLINGEDGE << CSL_MCASP_ACLKXCTL_CLKXP_SHIFT)|\
(CSL_MCASP_ACLKXCTL_ASYNC_SYNC << CSL_MCASP_ACLKXCTL_ASYNC_SHIFT)|\
(CSL_MCASP_ACLKXCTL_CLKXM_INTERNAL << CSL_MCASP_ACLKXCTL_CLKXM_SHIFT)|\
(0x03 << CSL_MCASP_ACLKXCTL_CLKXDIV_SHIFT);
//发送时钟检查控制寄存器
//mcasp0Regs->XCLKCHK = 0x00FF0008;//CSL_MCASP_XCLKCHK_RESETVAL; //CLKCHK0=0xFF000F; // Doesn't care

//发送高频时钟控制:外部时钟源;发送位流高频时钟极性:上升沿,不翻转;发送高频时钟分配比:2
mcasp0Regs->AHCLKXCTL = (CSL_MCASP_AHCLKXCTL_HCLKXM_INTERNAL << CSL_MCASP_AHCLKXCTL_HCLKXM_SHIFT)|\
(CSL_MCASP_AHCLKXCTL_HCLKXP_NOTINVERTED << CSL_MCASP_AHCLKXCTL_HCLKXP_SHIFT)|\
(0x01 << CSL_MCASP_AHCLKXCTL_HCLKXDIV_SHIFT);
//发送TDM时隙寄存器:slot0,slot1是活跃的
mcasp0Regs->XTDM = (Uint32) 0x03;

//发送中断控制寄存器:中断全部使能
mcasp0Regs->XINTCTL = 0x00000020;
mcasp0Regs->XCLKCHK = 0x00FF0008;
//EDMA EVENT GENERATE
//mcasp0Regs->REVTCTL = CSL_MCASP_REVTCTL_RDATDMA_RSV;

/******************串口配置***************************/

//AXR0[0],AXR0[1]为接收器
mcasp0Regs->SRCTL0 = (CSL_MCASP_SRCTL0_SRMOD_RCV << CSL_MCASP_SRCTL0_SRMOD_SHIFT);
//mcasp0Regs->SRCTL1 = (CSL_MCASP_SRCTL0_SRMOD_RCV << CSL_MCASP_SRCTL1_SRMOD_SHIFT);
//AXR0[5],AXR0[6]为发送器
mcasp0Regs->SRCTL6 = (CSL_MCASP_SRCTL6_SRMOD_XMT << CSL_MCASP_SRCTL6_SRMOD_SHIFT);
//mcasp0Regs->SRCTL0 = (CSL_MCASP_SRCTL0_SRMOD_XMT << CSL_MCASP_SRCTL0_SRMOD_SHIFT);

/*****LOOPBACK*****/


/*****配置输入输出引脚*****AXR00---输出,AXR01---输入**********/
// both transmit and receiver use the same FS and BCLK

//将MCASP0所有管脚均用做MCASP引脚
mcasp0Regs->PFUNC = CSL_MCASP_PFUNC_RESETVAL;
//mcasp0Regs->PDIR =0x1C000040;
//LOOPBACK
mcasp0Regs->PDIR =0x1C000001;

mcasp0Regs->DITCTL = 0x00000000; // Not used
mcasp0Regs->DLBCTL = 0x00000000; // Not used
mcasp0Regs->AMUTE = 0x00000000;

/************ Step 3: reset AHCLK **************/
//******a.Take the respective internal high-frequency serial clock divider(s) out of reset
mcasp0Regs->RGBLCTL = (CSL_MCASP_RGBLCTL_RHCLKRST_ACTIVE << CSL_MCASP_RGBLCTL_RHCLKRST_SHIFT);

//******b.Read back from GBLCTL to ensure the bit(s) to which you wrote are successfully latched in
//GBLCTL before you proceed.
while(!(mcasp0Regs->RGBLCTL & 0x0002));

//******a.Take the respective internal high-frequency serial clock divider(s) out of reset
mcasp0Regs->XGBLCTL |= (CSL_MCASP_XGBLCTL_XHCLKRST_ACTIVE << CSL_MCASP_XGBLCTL_XHCLKRST_SHIFT);

//******b.Read back from GBLCTL to ensure the bit(s) to which you wrote are successfully latched in
//GBLCTL before you proceed.
while(!(mcasp0Regs->XGBLCTL & 0x0200));

/************Step 4: reset ACLK **************/
//******a.Take the respective internal serial clock divider(s) out of reset

mcasp0Regs->RGBLCTL |= (CSL_MCASP_RGBLCTL_RCLKRST_ACTIVE << CSL_MCASP_RGBLCTL_RCLKRST_SHIFT);

//******b.Read back from GBLCTL
while(!(mcasp0Regs->RGBLCTL & 0x0001));

//******a.Take the respective internal serial clock divider(s) out of reset
mcasp0Regs->XGBLCTL |= (CSL_MCASP_XGBLCTL_XCLKRST_ACTIVE << CSL_MCASP_XGBLCTL_XCLKRST_SHIFT);

//******b.Read back from GBLCTL
while(!(mcasp0Regs->XGBLCTL & 0x0100));

//EDMA3_SendInitialCfg();
//EDMA3_ReceiveStartCfg();
//mcasp0Regs->RINTCTL = 0x00000020;

// Step 6: 激活串行器
mcasp0Regs->XSTAT = (Uint32) 0xFFFF;
mcasp0Regs->RSTAT = (Uint32) 0xFFFF;

//******b.Take the respective serializers out of reset
mcasp0Regs->XGBLCTL |= (CSL_MCASP_XGBLCTL_XSRCLR_ACTIVE << CSL_MCASP_XGBLCTL_XSRCLR_SHIFT);

//******c.Read back from GBLCTL
while(!(mcasp0Regs->XGBLCTL & 0x0400));

//******b.Take the respective serializers out of reset
mcasp0Regs->RGBLCTL |= (CSL_MCASP_RGBLCTL_RSRCLR_ACTIVE << CSL_MCASP_RGBLCTL_RSRCLR_SHIFT);

//******c.Read back from GBLCTL
while(!(mcasp0Regs->RGBLCTL & 0x0004));

//mcasp0Regs->XBUF6 = 0x89649548;
//mcasp0Regs->RBUF0 = 0x58755639;

// Step 8: 状态机退出复位

//******a.Take the respective state machine(s) out of reset
mcasp0Regs->RGBLCTL |= (CSL_MCASP_RGBLCTL_RSMRST_ACTIVE << CSL_MCASP_RGBLCTL_RSMRST_SHIFT);

//******b.Read back from GBLCTL
while(!(mcasp0Regs->RGBLCTL & 0x0008));

//******a.Take the respective state machine(s) out of reset
mcasp0Regs->XGBLCTL |= (CSL_MCASP_XGBLCTL_XSMRST_ACTIVE << CSL_MCASP_XGBLCTL_XSMRST_SHIFT);

//******b.Read back from GBLCTL
while(!(mcasp0Regs->XGBLCTL & 0x0800));

// Step 9 帧同步信息退出复位

//******a.Take the respective frame sync generator(s) out of reset
mcasp0Regs->RGBLCTL |= (CSL_MCASP_RGBLCTL_RFRST_ACTIVE << CSL_MCASP_RGBLCTL_RFRST_SHIFT);

//******b.Read back from GBLCTL
while(!(mcasp0Regs->RGBLCTL & 0x0010));

//******a.Take the respective frame sync generator(s) out of reset
mcasp0Regs->XGBLCTL |= (CSL_MCASP_XGBLCTL_XFRST_ACTIVE << CSL_MCASP_XGBLCTL_XFRST_SHIFT);

//******b.Read back from GBLCTL
while(!(mcasp0Regs->XGBLCTL & 0x1000));

interrupt void Interrupt4(void)
{

mcasp0Regs->RSTAT |= 0x20;
ICR = 0x10;

rcv[cnt++]= mcasp0Regs->RBUF0 ;
if(cnt>=64)
cnt=0;
}

  • Hi Xian,

    Thanks for your post.

    As per the value of  rstat (0x171) posted above, it states that, the ROVRN (receiver overrun) had occured which indicates that, the previous data of RBUF is not yet been serviced by the CPU/DMA inspite receive data ready flag (RDATA) bit  is set in RSTAT/RINTCTL currently and is being ready to transfer data from XRSR to RBUF & being serviced by CPU/DMA but instead, it sets the ROVRN flag due to the cause of the receive interrupt (RINT) and failed to cause the DMA Rx. event (AREVT).

    In my opinion, there is a typical sequential order involved in McASP configuration, even to clear the respective transmitter and receiver status registers by writing XSTAT = FFFFh and RSTAT = FFFFh, it should be done only before activating the configured Tx. & Rx. serializers else, it wouldn't clear the Rx/Tx status registers (RSTAT/XSTAT) appropriately as expected.

    Kindly ensure the sequential order involved in configuring the McASP initialization steps as mentioned in Section 26.2.4.1.2 in omapl137 TRM as below:

    http://www.ti.com/lit/ug/spruh92b/spruh92b.pdf

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    -------------------------------------------------------------------------------------------------------

     

  • Hello Sivaraj ,

    Thanks for your replying.

    I am sure the sequential order involved in configuring the McASP initialization steps is right,bucause I checked many times,but I can't receive any data in RBUF0 in interrupt function.Could you help me check the interrupt function for receiving?And I have configured the McASP to loopback mode,but still not data be received,how to explain this?

    Thinks.

    xw shen