This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ARP packet storm with AM335x

Hi,


I have 2 am335x devices on hand, each one has 2 LAN port. (as the following figure)


Network topology:

                                     LAN 1

  • Device A <-----------------> Device B
  • Device A LAN 2 : loopback jig
  • Device B LAN 2 : loopback jig

I find that It will cause ARP strom to destroy the operation of local network only if the loopback jig is plugged before booting up.

But if I wait the booting progress finished and plug the loopback jig, there is no any abnormal situation!

Is this a CPU limitation ?

OS: Linux AM335xPSP_04.06.00.11

Thanks for any advice.