This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to pause XGE transmission?

Hi

We are working with a Keystone2 device. We communicate with another device using the XGE 10Gbe interface. If the remote device fails the system switches to another remote device. During the handover from one device to the other we need to pause transmission.   While transmission is paused,, the application may continue to send UDP packets to the XGE interface.   These packets should queue until the interface is unpaused.


How could I pause transmission for this purpose? Can I do so in the XGE interface,  or is there something I could do in the QMSS or in the PKT DMA?

Best regards

David