I have the following error when i tried to boot with SD card.Unfortunately I already erased the Nand Flash and
Texas Instruments X-Loader 1.41
Starting on with MMC
Unsupported Chip!
Reading boot sector
275904 Bytes Read from MMC
Starting OS Bootloader from MMC...
U-Boot 2009.01-dirty (Feb 19 2009 - 12:23:21)
I2C: ready
OMAP3530-GP rev 2, CPU-OPP2 L3-165MHz
OMAP3 Beagle board + LPDDR/NAND
DRAM: 128 MB
NAND: No NAND device found!!!
0 MiB
How do i get a compatible X-Loader.
Is the problem with "No Nand device found" Hardware related???