hi all ,now when i create the dec link ,i set the below parameter
decPrm.chCreateParams[i].algCreateStatus = DEC_LINK_ALG_CREATE_STATUS_DONOT_CREATE;
so i can call the function Vdec_createChn() to create a dec channel direactly
then now i found the i can disable a dec channel ,but if i call the enable function to enable the disable dec channel ,that can not enable dec?so why?