Hi,
i'm trying to create the sample demo in
http://processors.wiki.ti.com/index.php/TI-RTOS_HTTP_Example
and it is working but the my board is taking the IP using the DHCP and sometimes not, after more investigation using the wireshark and listening to the traffic from the board, i found that the board takes an IP address when it broadcast the request to the DHCP server and it won't get the IP and displaying fault message when it doesn't broadcast the request ""Service Status: DHCPC : Enabled : Fault : 002""
So why sometimes the board isn't broadcasting the DHCP request?
my board is: DK-TM4C129
the NDK version :ndk_2_23_00_00
the TI-RTOS version:tirtos_1_21_00_09
Thanks,
Mohamed Fawzy