This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 Errata GPIO Bank 1 Interrupt Question



I have some questions regarding the GPIO Bank 1 interrupt on the DM648 device.  I have read the section in the DM648 errata as well as this forum post : (http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/t/6666.aspx?PageIndex=1).  I can't seem to distinguish exactly what the problem is with the GPIO bank 1 interrupt between what this post is saying, what the errata says, and the behavior of my system.

The errata states that no interrupt will be generated for a GPIO bank 1 signal.  This forum post seems to say that an erroneous interrupt is generated for the GPIO bank 1 interrupt selection number (42).  My system (I am using GPIO16 and GPIO1 for my interrupts) behaves in a way where both of my ISRs are being serviced.  I really need to know what exactly the problem is with the GPIO bank 1 interrupts.  I cannot tell for sure whether or not my GPIO16 ISR is running at the desired moment or if it is being erroneously generated because of a silicon error.  Any help is really appreciated.

Thanks,

Jason