Hi TI,
My task is to make OMAP4430 receive a data from FPGA over the CCP2 camera interface, throughput > 100Mb/sec.
FPGA acts here as a camera sensor following "SMIA 1.0 Part 2: CCP2 Specification".
Problem I experience here is initialisation of the OMAP4430 CCP2 interface.
I found the Technical Reference Manual a bit unclear regarding CCP2 initialisation, and I need some clarification:
- Is the MIPI HS BYTECLK clock needed in CCP2 mode in order to have RESET_DONE set?
This is highlighted for CSI2 but not for CPP2, see 8.2.3.2.2 ISS CSI2 PHY and Link Initialization Sequence, it says CAUTION For the CSI2_COMPLEXIO_CFG[29] RESET_DONE bit to be set to 0x1 (reset completed), the external sensor must to be active and sending the MIPI HS BYTECLK.
- Could someone let me know is there any available code which does a full CCP2 initialisation.
Kind Regards
Dragan