This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with UART on DM6437 EVM

I'm using the DM6437 and trying to connect to my computer through the UART RS-232 interface.  I have connected the P8 port with a straight-through db9 cable to a serial to USB adapter(link).

I am running the functions EVMDM6437_UART_open, EVMDM6437_UART_put_char from the loopback test sample code to try to write data out.  On my computer, I have tried running teraterm and several other serial terminals, but I am not seeing any data written.  I am pretty sure that the driver is set up correctly, and I have changed the settings to match the ones given to the DSP (baud rate = 9600, no parity, etc).  

Is there any reason this shouldn't be working correctly?  Should I be using a null modem cable instead?  Do I need to attach the daughtercard to use the UART interface?  Any help is appreciated!