This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why dm8168 syslink example run error?

uboot arg:

setenv bootargs console=ttyO2,115200n8 rootwait rw mem=169M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti816xfb.vram=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=${serverip}:/root/targetfs ip=192.168.10.202:192.168.10.2:192.168.10.2:255.255.255.0:dm8168:eth0:off

Linux:

root@dm816x-evm:/media/net/home# ./unloadfirmware.sh
Unloading HDVICP2 Firmware
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
Firmware Loader debugging not configured
Default FL_DEBUG: warning
Allowed FL_DEBUG levels: error, warning, info, debug, log
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: 1 stop Successful
Unloading HDVPSS Firmware
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
Firmware Loader debugging not configured
Default FL_DEBUG: warning
Allowed FL_DEBUG levels: error, warning, info, debug, log
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: 2 stop Successful
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
Firmware Loader debugging not configured
Default FL_DEBUG: warning
Allowed FL_DEBUG levels: error, warning, info, debug, log
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: 0 start Successful
root@dm816x-evm:/media/net/home# modprobe syslink
root@dm816x-evm:/media/net/home#cd /usr/share/ti/syslink-examples/TI816X/helloworld
root@dm816x-evm:/media/net/usr/share/ti/syslink-examples/TI816X/helloworld# ./ru
n.sh
+ ./slaveloader startup DSP server_dsp.xe674
Attached to slave procId 0.
Loading procId 0.
Loaded file server_dsp.xe674 on slave procId 0.
Started slave procId 0.
+ ./app_host DSP
notify_shm_drv_sendevent failed! status = 0xfffffff2
notify_send_event failed! status = 0xfffffff2+ ./slaveloader shutdown DSP
Stopped slave procId 0.
Unloaded slave procId 0.
Detached from slave procId 0.
root@dm816x-evm:/media/net/usr/share/ti/syslink-examples/TI816X/helloworld#

root@dm816x-evm:/media/net/usr/share/ti/syslink-examples/TI816X/messageq# ./run.
sh
+ ./slaveloader startup DSP server_dsp.xe674
Attached to slave procId 0.
Loading procId 0.
Loaded file server_dsp.xe674 on slave procId 0.
Started slave procId 0.
+ ./app_host DSP
--> main:
--> Main_main:
Main_main: load callback failed
<-- Main_main:
<-- main:
+ ./slaveloader shutdown DSP
Stopped slave procId 0.
Unloaded slave procId 0.
Detached from slave procId 0.
root@dm816x-evm:/media/net/usr/share/ti/syslink-examples/TI816X/messageq#