Hi all,
i am a "new bee" with these DaVinci processors and am using DM388 RDK for some project of my own and i want to make a simple chain usecase which consists CAPTURE_GLBCE_ISP_SCALAR_DISPLAY links in a row.....I properly know that how to connect links by giving the previous link and next link in its parameters and i have implemented it with USECASE (CAPTURE_MCTNF_SCALAR_DISPLAY) but i cant get the streaming over the HDMI in this usecase..also i get the successful logs of streaming in linux console...
can anyone help me out on this streaming issue and also to execute the first usecase i mentioned ,which things i have to take care or should i just connect the links,start links and it will start working ..
and can we shuffle the links ( scalar,dei, SwMs etc) between CAPTURE and DISPLAY...will it work or not...
and kindly refer me a document which shows the proper working of these IPCbitsInRTOS and HLOS
,IPCFramesOUT and IN...if it is in RDK Given by you ,tell me the location of it...
it will be very helpful for me to grab these things for which i am very excited...reply soon as anyone can....
thanks in advance.. :)