This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

installing perl in ARM

Hi TI ,

            I am installing Perl5.18.2 in Target Board(ARM) and Download Perl5.18.2..i went to Directory Path.

         -> project/ti-sdk-am335x-evm-06.00.00.00/example-applications/Apps/perl-5.18.2

            cd Cross means  project/ti-sdk-am335x-evm-06.00.00.00/example-applications/Apps/perl-5.18.2/Cross

      After change the Config file

     After make patch

   After make perl    and then Coming Error

i send log file and Plz solve my problem.............

......................

..................

`sh  cflags "optimize='-O2'" perlmini.o` -fexpensive-optimizations -fomit-frame-pointer -O2 -march=armv4 -mtune=strongarm1100 -mapcs-32 -DPERL_IS_MINIPERL -DPERL_EXTERNAL_GLOB perlmini.c
      CCCMD =  arm-linux-gcc -DPERL_CORE -c  -fexpensive-optimizations -fomit-frame-pointer -O2 -march=armv4 -mtune=strongarm1100 -mapcs-32  -O2 -Wall
/bin/sh: arm-linux-gcc: not found
make[1]: *** [perlmini.o] Error 127
make[1]: Leaving directory `/home/mistral/project/ti-sdk-am335x-evm-06.00.00.00/example-applications/Apps/perl-5.18.2'
make[1]: Entering directory `/home/mistral/project/ti-sdk-am335x-evm-06.00.00.00/example-applications/Apps/perl-5.18.2'
make[1]: *** No rule to make target `more'.  Stop.
make[1]: Leaving directory `/home/mistral/project/ti-sdk-am335x-evm-06.00.00.00/example-applications/Apps/perl-5.18.2'
make: *** [perl] Error 2