Hi folks,
I'm using ISS 3.5 and EZSDK 5.05 on a DM8127 platform. I am capturing a 1936x1936 image on the ISS and I want to create two streams from it, one outputting a 1936x1936 size image and one outputting a 960x960 image stream.
My understanding is that the ISS contains two resizers and the plan is to use both of these resizers with one stream putting the resizer in bypass mode (RSZA) and the other stream enabling the resizer (RSZB).
As a test I have modified one of the OMX IL examples to just capture from the ISS and dump the captured frames to a file.
When I have a single stream from the ISS enabled (via a bypassed resizer A), this works fine and video received in the file is perfect. However, when I enable the second stream on the ISS (again bypassing the reisizer B), I am finding that the video output on both streams becomes purple.
At the moment, I am not able to fix this.
Is it valid to use the ISS to produce two streams using both resizers?
Has anyone come across a similar problem?
Any help would be appreciated,
Thanks in advance,
Regards,
Terry