Other Parts Discussed in Thread: CCSTUDIO
Hi,
I have a problem in my DSP C54x power supply.
In my board [PCB designed around C5402 DSP]. I have a voltage regulator that delivers CVDD=1.8V and DVDD=3.3V voltages for DSP power supply.
I was able to run/debug programs, but after while, some problem occurred. [unfortunately-as yet- I don’t know what is exactly the source of problem].
anyway, now the main problem is that CVDD and DVDD connections are tied. As a result:
- I can't connect Emulator to the board
- I measured CVDD=DVDD=3.3V.
- when DSP powered, the XF and HRDY signals =3.3V.
- I verified that problems doesnt come from the voltage regulator(now removed from the PCB).
My questions:
1. I want to verify if the problem of connection between CVDD and DVDD comes from the DSP itself. It’s possible?
2. what could happen if the DSP has powered with CVDD=DVDD=3.3V?
your suggestions to solve my problem will be appreciated.