Other Parts Discussed in Thread: TPS65920, OMAP3530, OMAP3503, TPS65950
Hello. I am designing a portable system that will use the OMAP3530 and the TPS65920. I have no audio in this application so I am not limited to the 26 MHz usually required in these situations. I need to minimize power consumption as much as possible, hence I have several questions about the clock source and frequency between these two ICs. Please answer all of my questions, if possible, but they all boil down to this question:
1) Is it better from both a power savings AND performance perspective, to have the OMAP3530 or the TPS65920 as the clock master? If the OMAP3530 as the clock master is the better option, is it better to use a crystal, CMOS clock source or clock squarer source, and at what frequency?
The nitty-gritty details questions:
2) If TPS65920 is the clock master, it requires either a 19.2 MHz, 26 MHz, or 38.4 MHz HFCLKIN (sine wave or square wave clock, not a crystal). Is there any power savings in using a sine wave input clock vs. a square wave input clock?
3) If the OMAP3530 is the clock master, it may be either a crystal, CMOS digital clock, or a clock squarer source. Of these three, is there any power savings in using one vs. another? Can you give a relative ranking of these three as far as power savings?
4) The OMAP3530 may use crystals ranging from 12 MHz to 19.2 MHz. Is there any benefit to using a faster crystal vs. a slower one? With the flexible range of the DPLL circuits it is possible to generate the fastest ARM and DPS clocks from even a 12 MHz crystal.
5) As far as the OMAP3530 / TPS65920 power saving modes (e.g., sleep, performance points [OPP], etc.) does having the OMAP3530 as the clock master result in any reduced power saving modes by the TPS65920?
6) From a performance standpoint, is it better to have the TPS65920 as the clock master or the OMAP3530?
6) From a power savings standpoint, is it better to have the OMAP3530 as the clock master or the TPS65920?
7) If the OMAP3530 as the clock master is the better option, is it better to use a crystal or a clock source, and at what frequency?
8) Is there any downsides, or points I am missing in the above question list?
Thanks!
Charles