This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Source code of mcsdk_linux packages?

Hello,


I am working on KeyStone II device, and by now I need the source code of the images that contained in the MCSDK package to be able to recompíle them. I already searched all the package but I couldnt find the source codes of:

uImage-k2hk-evm.dtb

uImage-keystone-evm.bin

uImage-rt-k2hk-evm.dtb

uImage-rt-keystone-evm.bin

Im using mcsdk_linux_3_00_03_15, and  gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux for cross-compilation.


Thanks in advance for the help.

Ronny