This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Patch: fix bitbanding bug in usbdbulk.c



This is the way it's already done in usbdhid.c and usbdcdc.c so I just copied that code.  Without it, you either get an exception (if the "bitbanding" address is outside of the memory space mapped in the MMU) or a memory overwrite (depending on your DDR size, due to memory aliasing).

//*****************************************************************************
+//This macro is used to diable the bit band operartion. Need to undefine this macro to use the
+// bit band operation.
+//***************************************************************************
+#define DISABLE_BIT_BAND
+
+//*****************************************************************************
//

[...] 

SetDeferredOpFlag(volatile unsigned short *pusDeferredOp, unsigned short usBit,
tBoolean bSet)
{
+#ifdef DISABLE_BIT_BAND
+    if(bSet)
+    {
+        HWREG(pusDeferredOp) |= (1<<usBit);
+    }
+    else
+    {
+        HWREG(pusDeferredOp) &= ~(1<<usBit);
+    }
+#else
     //
     // Set the flag bit to 1 or 0 using a bitband access.
     //
     HWREGBITH(pusDeferredOp, usBit) = bSet ? 1 : 0;
+#endif
}

Thanks,

Orjan