The VDDA3P3V_USB0 pulls up to 0.836V when only the USB0_VBUS is supplied in the customer boards, also it can show in the EVM. In the EVM, the VDDA3P3V_USB0 (J31_2) pulls up to 0.627V when only the VUSB_VBUS0(J36_1) is supplied 5V by an external supply.
Is there the internal leakage current path from the USB0_VBUS to the VDDA3P3V_USB0?
Best regards,
Daisuke