This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 Enclink

I want to use two enc link Instance in ipnc rdk 3.5, because there are some special functions to complete.

For example, I want to complete the flow as follow:

EncLink0 ID is SYSTEM_LINK_ID_VENC_0, and  EncLink1 ID is SYSTEM_LINK_ID_VENC_1.

In the flow, If I do not use EncLink1, IPCM3IN1->NULL, the program running is OK. But if I add the EncLink1, and the params of Enclink1 are the same as the EncLink0,  the program running is "time out exit".

What  causes the error?