Hello,
We are using TMS320DM8168 Video out interface, and have following queries:
1) If VOUT0_CLK pin, clock edge programmable to be rising or falling edge? In datasheet page 266, timing is shown as w.r.t. rising edge only. Pls confirm.
2) What are the VOUT interface clock and data load conditions? IBIS model indicates load for all temperature corners as 100M-ohm and 15pF.
3) Datasheet page 256, table 8-72, sub-note 2, states minimum delay time = Tc * 0.27; is this valid for all temperature corners for same load at all temperature corners or will this vary. If varies, pls let us know for typical, slow and fast corner the minimum delay time.
Pls do revert on this at the earliest.
Thanks & Regards,
Roma Bhagat