This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 AEWB problem

Hello everybody!

We have streaming application running on 2.6.32 kernel.
It's based on DMAI example. It generates RTP stream, uses Appro AEWB library and LDC correction.
We are changing stream resolution (1280/640/320) without program exit.
When I run AEWB in main loop it works OK.
When I run it in separate thread (triggered in the same place) after N resolution changes video is white (max dgain, max exposure, max brightness...).
It must be problem with dm368 because only HW reset helps.

Maybe You would know what cause this problem?
Thanks for help!

Tomek