This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 voice encode failure on internal voice codec.



Hi there

EVM : Spectrum Digital EVM

LSP version : 2.10.01.18

DVSDK Version : 2.10.01.18

I'm going to use the internal voice codec of Dm365.

Currently the voice enc/dec is ok with external AIC3x codec.

But when i re-configured the kernel to use the internal voice codec and tried enc/dec.

In this case decode is ok but the encode has a problem like below message.

Encode demo started.
Error: Failed to encode speech buffer
Is there anybody who succeed in encoding voice using internal voice codec of DM365
Thanks