This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5.5 opens app.cfg with XDC runtime error: too many arguments

Other Parts Discussed in Thread: TMS320C6748, CDCE913, TVP5147, CCSTUDIO

Hello E2E Community,

I have a SYS/BIOS application that has being working for over 5 months and have being modifying and building my application since without any problems.  Today I needed to add a new task to the application so I double clicked the app.cfg file and when CCS loads the file into the SYS/BIOS window, it showed an error in the 'Problems' window.  At this point, when I select the Task tab, all my tasks are in the Task list box but the settings are all at default and not what is in the app.cfg file.

Description                                                     Resource      Path                                   Location
XDC runtime error: too many arguments       app.cfg          /edge_video_analytics      Configuration Validation

Type
XDCTools Configuration Marker

I am not sure where the problem is in the app.cfg file.  Can someone give me some guidance as to how to debug this error message and how to fix it.  I am using CCSv5.5, compiler version TI v7.4.6,  SYS/BIOS 6.35.4.50, and the application runs on a TMS320C6748 DSP.

Thanks,
JumpStart

  • Did you change any versions of CCS, SYS/BIOS, XDCtools or codegen? Can you attach your .cfg file? If not, can you "friend" me and send it to me?

    Todd

  • Hello Todd,

    A month back I had a previous built error message (I don't remember what it is now) and I found on the E2E Community a thread that recommended I installed ti_cft_c6000_7.4.6_setup_win32 which resolved that previous problem.

    I was originally using Compiler version TI v7.4.4.  I have tried going back to the older version but still get the same error.

    I even went as far as to incrementally comment out sections of the .cfg file until the whole .cfg was commented out but still see the same error message.7206.app.cfg

    Thanks,
    JumpStart

  • I think I saw errors like that before. In some cases cleaning the project and rebuilding would help, but if not, then the problem is usually in some extra characters on the command line that runs configuration. Could you go to Project Properties->CCS Build->XDCtools->Advanced Options, and turn on "Show details during build"? Then, clean and rebuild and post the complete content of the output console.

  • Hello Sasha,

    Cleaning and rebuilding the project without turning on "Show details during build" show no error and no warnings.  When I turned on "Show details during build" I see one error message.  Below is the error message and the build output.

    Error
       package/cfg/app_pe674cfg.cmd\)\                     .xdchelp            /edge_video_analytics              C/C++ Problem

    **** Build of configuration Release for project edge_video_analytics ****

    "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all

    'Building file: ../app.cfg'

    'Invoking: XDCtools'

    "C:/ti/xdctools_3_25_03_72/xs" --xdcpath="C:/ti/bios_6_35_04_50/packages;C:/ti/ccsv5/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C674 -p ti.platforms.evm6748 -r release -c "C:/ti/ccsv5/tools/compiler/c6000_7.4.6" --compileOptions "-g --optimize_with_debug" -v "../app.cfg"

    #

    # making package.mak (because of package.bld) ...

    C:/ti/xdctools_3_25_03_72/xs  -Dxdc.path="C:/ti/bios_6_35_04_50/packages;C:/ti/ccsv5/ccs_base;C:/ti/xdctools_3_25_03_72/packages;.." -Dxdc.root=C:/ti/xdctools_3_25_03_72 -Dxdc.hostOS=Windows -Dconfig.importPath=".;C:/ti/bios_6_35_04_50/packages;C:/ti/ccsv5/ccs_base;C:/ti/xdctools_3_25_03_72/packages;..;C:/ti/xdctools_3_25_03_72;C:/ti/xdctools_3_25_03_72/etc" -Dxdc.bld.targets="" -DTOOLS=   -f C:/ti/xdctools_3_25_03_72/packages/xdc/bld/bld.js ./config.bld package.bld package.mak

    #

    # generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...

    C:/ti/xdctools_3_25_03_72/xs -Dxdc.path="C:/ti/bios_6_35_04_50/packages;C:/ti/ccsv5/ccs_base;C:/ti/xdctools_3_25_03_72/packages;.." -Dxdc.root=C:/ti/xdctools_3_25_03_72 -Dxdc.hostOS=Windows -Dconfig.importPath=".;C:/ti/bios_6_35_04_50/packages;C:/ti/ccsv5/ccs_base;C:/ti/xdctools_3_25_03_72/packages;..;C:/ti/xdctools_3_25_03_72;C:/ti/xdctools_3_25_03_72/etc" -Dxdc.bld.targets="" -DTOOLS=  -f xdc/services/intern/cmd/build.xs  -m package/package.xdc.dep -i package/package.xdc.inc package.xdc

    #

    # configuring app.xe674 from package/cfg/app_pe674.cfg ...

    C:/ti/xdctools_3_25_03_72/xs -Dxdc.path="C:/ti/bios_6_35_04_50/packages;C:/ti/ccsv5/ccs_base;C:/ti/xdctools_3_25_03_72/packages;.." -Dxdc.root=C:/ti/xdctools_3_25_03_72 -Dxdc.hostOS=Windows -Dconfig.importPath=".;C:/ti/bios_6_35_04_50/packages;C:/ti/ccsv5/ccs_base;C:/ti/xdctools_3_25_03_72/packages;..;C:/ti/xdctools_3_25_03_72;C:/ti/xdctools_3_25_03_72/etc" -Dxdc.bld.targets="" -DTOOLS=   xdc.cfg app.xe674 package/cfg/app_pe674.cfg package/cfg/app_pe674

    C:/ti/xdctools_3_25_03_72/bin/sed 's"^\"\(package/cfg/app_pe674cfg.cmd\)\""\"C:/Vantage/TMS320C6748/demos/edge_video_analytics/Release/configPkg/\1\""' package/cfg/app_pe674.xdl > linker.cmd

    C:/ti/xdctools_3_25_03_72/bin/rm -f package/cfg/app_pe674.oe674

    #

    # cle674 package/cfg/app_pe674.c ...

    C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x -c  -g --optimize_with_debug -qq -pdsw225 -mo -mv6740 --abi=eabi -eo.oe674 -ea.se674  --embed_inline_assembly  -Dxdc_cfg__header__='configPkg/package/cfg/app_pe674.h'  -Dxdc_target_name__=C674 -Dxdc_target_types__=ti/targets/elf/std.h -Dxdc_bld__profile_release -Dxdc_bld__vers_1_0_7_4_6 -O2  -I. -IC:/ti/bios_6_35_04_50/packages -IC:/ti/ccsv5/ccs_base -IC:/ti/xdctools_3_25_03_72/packages -I.. -IC:/ti/ccsv5/tools/compiler/c6000_7.4.6/include -fs=./package/cfg -fr=./package/cfg -fc package/cfg/app_pe674.c

    C:/ti/xdctools_3_25_03_72/bin/mkdep -a package/cfg/app_pe674.oe674.dep -p package/cfg -s oe674 package/cfg/app_pe674.c -C   -g --optimize_with_debug -qq -pdsw225 -mo -mv6740 --abi=eabi -eo.oe674 -ea.se674  --embed_inline_assembly  -Dxdc_cfg__header__='configPkg/package/cfg/app_pe674.h'  -Dxdc_target_name__=C674 -Dxdc_target_types__=ti/targets/elf/std.h -Dxdc_bld__profile_release -Dxdc_bld__vers_1_0_7_4_6 -O2  -I. -IC:/ti/bios_6_35_04_50/packages -IC:/ti/ccsv5/ccs_base -IC:/ti/xdctools_3_25_03_72/packages -I.. -IC:/ti/ccsv5/tools/compiler/c6000_7.4.6/include -fs=./package/cfg -fr=./package/cfg

    'Finished building: ../app.cfg'

    ' '

    'Building file: ../AlgoDayNight.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="AlgoDayNight.pp" --cmd_file="./configPkg/compiler.opt"  "../AlgoDayNight.c"

    'Finished building: ../AlgoDayNight.c'

    ' '

    'Building file: ../adv7343.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="adv7343.pp" --cmd_file="./configPkg/compiler.opt"  "../adv7343.c"

    'Finished building: ../adv7343.c'

    ' '

    'Building file: ../algoUtils.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algoUtils.pp" --cmd_file="./configPkg/compiler.opt"  "../algoUtils.c"

    'Finished building: ../algoUtils.c'

    ' '

    'Building file: ../algobike.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algobike.pp" --cmd_file="./configPkg/compiler.opt"  "../algobike.c"

    'Finished building: ../algobike.c'

    ' '

    'Building file: ../algobindata.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algobindata.pp" --cmd_file="./configPkg/compiler.opt"  "../algobindata.c"

    'Finished building: ../algobindata.c'

    ' '

    'Building file: ../algoconfig.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algoconfig.pp" --cmd_file="./configPkg/compiler.opt"  "../algoconfig.c"

    'Finished building: ../algoconfig.c'

    ' '

    'Building file: ../algodet.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algodet.pp" --cmd_file="./configPkg/compiler.opt"  "../algodet.c"

    'Finished building: ../algodet.c'

    ' '

    'Building file: ../algofog.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algofog.pp" --cmd_file="./configPkg/compiler.opt"  "../algofog.c"

    'Finished building: ../algofog.c'

    ' '

    'Building file: ../algointerface.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algointerface.pp" --cmd_file="./configPkg/compiler.opt"  "../algointerface.c"

    'Finished building: ../algointerface.c'

    ' '

    'Building file: ../algolane.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algolane.pp" --cmd_file="./configPkg/compiler.opt"  "../algolane.c"

    'Finished building: ../algolane.c'

    ' '

    'Building file: ../algolearn.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algolearn.pp" --cmd_file="./configPkg/compiler.opt"  "../algolearn.c"

    'Finished building: ../algolearn.c'

    ' '

    'Building file: ../algolearndiag.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algolearndiag.pp" --cmd_file="./configPkg/compiler.opt"  "../algolearndiag.c"

    'Finished building: ../algolearndiag.c'

    ' '

    'Building file: ../algolntrack.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algolntrack.pp" --cmd_file="./configPkg/compiler.opt"  "../algolntrack.c"

    'Finished building: ../algolntrack.c'

    ' '

    'Building file: ../algolntrackdiag.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algolntrackdiag.pp" --cmd_file="./configPkg/compiler.opt"  "../algolntrackdiag.c"

    'Finished building: ../algolntrackdiag.c'

    ' '

    'Building file: ../algomain.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algomain.pp" --cmd_file="./configPkg/compiler.opt"  "../algomain.c"

    'Finished building: ../algomain.c'

    ' '

    'Building file: ../algoproc.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algoproc.pp" --cmd_file="./configPkg/compiler.opt"  "../algoproc.c"

    'Finished building: ../algoproc.c'

    ' '

    'Building file: ../algotrack.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algotrack.pp" --cmd_file="./configPkg/compiler.opt"  "../algotrack.c"

    'Finished building: ../algotrack.c'

    ' '

    'Building file: ../algovehicle.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algovehicle.pp" --cmd_file="./configPkg/compiler.opt"  "../algovehicle.c"

    'Finished building: ../algovehicle.c'

    ' '

    'Building file: ../algovirtualzone.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algovirtualzone.pp" --cmd_file="./configPkg/compiler.opt"  "../algovirtualzone.c"

    'Finished building: ../algovirtualzone.c'

    ' '

    'Building file: ../algozone.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="algozone.pp" --cmd_file="./configPkg/compiler.opt"  "../algozone.c"

    'Finished building: ../algozone.c'

    ' '

    'Building file: ../cbcr422sp_to_rgb565_dsp.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="cbcr422sp_to_rgb565_dsp.pp" --cmd_file="./configPkg/compiler.opt"  "../cbcr422sp_to_rgb565_dsp.c"

    'Finished building: ../cbcr422sp_to_rgb565_dsp.c'

    ' '

    'Building file: ../cdce913.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="cdce913.pp" --cmd_file="./configPkg/compiler.opt"  "../cdce913.c"

    'Finished building: ../cdce913.c'

    ' '

    'Building file: ../channel.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="channel.pp" --cmd_file="./configPkg/compiler.opt"  "../channel.c"

    'Finished building: ../channel.c'

    ' '

    'Building file: ../clock.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="clock.pp" --cmd_file="./configPkg/compiler.opt"  "../clock.c"

    'Finished building: ../clock.c'

    ' '

    'Building file: ../codecif.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="codecif.pp" --cmd_file="./configPkg/compiler.opt"  "../codecif.c"

    'Finished building: ../codecif.c'

    ' '

    'Building file: ../command.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="command.pp" --cmd_file="./configPkg/compiler.opt"  "../command.c"

    'Finished building: ../command.c'

    ' '

    'Building file: ../config.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="config.pp" --cmd_file="./configPkg/compiler.opt"  "../config.c"

    'Finished building: ../config.c'

    ' '

    'Building file: ../dpr.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="dpr.pp" --cmd_file="./configPkg/compiler.opt"  "../dpr.c"

    'Finished building: ../dpr.c'

    ' '

    'Building file: ../frame.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="frame.pp" --cmd_file="./configPkg/compiler.opt"  "../frame.c"

    'Finished building: ../frame.c'

    ' '

    'Building file: ../hemisphere.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="hemisphere.pp" --cmd_file="./configPkg/compiler.opt"  "../hemisphere.c"

    'Finished building: ../hemisphere.c'

    ' '

    'Building file: ../i2cgpio.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="i2cgpio.pp" --cmd_file="./configPkg/compiler.opt"  "../i2cgpio.c"

    'Finished building: ../i2cgpio.c'

    ' '

    'Building file: ../isl59601.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="isl59601.pp" --cmd_file="./configPkg/compiler.opt"  "../isl59601.c"

    'Finished building: ../isl59601.c'

    ' '

    'Building file: ../led.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="led.pp" --cmd_file="./configPkg/compiler.opt"  "../led.c"

    'Finished building: ../led.c'

    ' '

    'Building file: ../main.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="main.pp" --cmd_file="./configPkg/compiler.opt"  "../main.c"

    'Finished building: ../main.c'

    ' '

    'Building file: ../memio.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="memio.pp" --cmd_file="./configPkg/compiler.opt"  "../memio.c"

    'Finished building: ../memio.c'

    ' '

    'Building file: ../memory.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="memory.pp" --cmd_file="./configPkg/compiler.opt"  "../memory.c"

    'Finished building: ../memory.c'

    ' '

    'Building file: ../option.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="option.pp" --cmd_file="./configPkg/compiler.opt"  "../option.c"

    'Finished building: ../option.c'

    ' '

    'Building file: ../sensitivity.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="sensitivity.pp" --cmd_file="./configPkg/compiler.opt"  "../sensitivity.c"

    'Finished building: ../sensitivity.c'

    ' '

    'Building file: ../serial.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="serial.pp" --cmd_file="./configPkg/compiler.opt"  "../serial.c"

    'Finished building: ../serial.c'

    ' '

    'Building file: ../snapshot.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="snapshot.pp" --cmd_file="./configPkg/compiler.opt"  "../snapshot.c"

    'Finished building: ../snapshot.c'

    ' '

    'Building file: ../subsample.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="subsample.pp" --cmd_file="./configPkg/compiler.opt"  "../subsample.c"

    'Finished building: ../subsample.c'

    ' '

    'Building file: ../tvp5147.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="tvp5147.pp" --cmd_file="./configPkg/compiler.opt"  "../tvp5147.c"

    'Finished building: ../tvp5147.c'

    ' '

    'Building file: ../uart_alt.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="uart_alt.pp" --cmd_file="./configPkg/compiler.opt"  "../uart_alt.c"

    'Finished building: ../uart_alt.c'

    ' '

    'Building file: ../uart_dpr.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="uart_dpr.pp" --cmd_file="./configPkg/compiler.opt"  "../uart_dpr.c"

    'Finished building: ../uart_dpr.c'

    ' '

    'Building file: ../uart_local.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="uart_local.pp" --cmd_file="./configPkg/compiler.opt"  "../uart_local.c"

    'Finished building: ../uart_local.c'

    ' '

    'Building file: ../ustdlib.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="ustdlib.pp" --cmd_file="./configPkg/compiler.opt"  "../ustdlib.c"

    'Finished building: ../ustdlib.c'

    ' '

    'Building file: ../utils.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="utils.pp" --cmd_file="./configPkg/compiler.opt"  "../utils.c"

    'Finished building: ../utils.c'

    ' '

    'Building file: ../videosync.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="videosync.pp" --cmd_file="./configPkg/compiler.opt"  "../videosync.c"

    'Finished building: ../videosync.c'

    ' '

    'Building file: ../vpifapp.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="vpifapp.pp" --cmd_file="./configPkg/compiler.opt"  "../vpifapp.c"

    'Finished building: ../vpifapp.c'

    ' '

    'Building file: ../wholesceneanalysis.c'

    'Invoking: C6000 Compiler'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/grlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/c674x/c6748" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/include/hw" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/nandlib/include" --include_path="C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/usblib/include" --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 --preproc_with_compile --preproc_dependency="wholesceneanalysis.pp" --cmd_file="./configPkg/compiler.opt"  "../wholesceneanalysis.c"

    'Finished building: ../wholesceneanalysis.c'

    ' '

    'Building target: edge_video_analytics.out'

    'Invoking: C6000 Linker'

    "C:/ti/ccsv5/tools/compiler/c6000_7.4.6/bin/cl6x" -mv6740 --abi=eabi -Ooff --define=c6748 --define=__NOVADOT --define=__EDGE4 --define=__EDGE5 --display_error_number --diag_warning=225 -z --stack_size=0x800 -m"edge_video_analytics.map" --heap_size=0x800 -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.6/lib" -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.6/include" -i"C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/binary/c674x/cgt_ccs/c6748/lcdkC6748/platform/Release" -i"C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/binary/c674x/cgt_ccs/c6748/drivers/Release" -i"C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/binary/c674x/cgt_ccs/c6748/system_config/Release" -i"C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/binary/c674x/cgt_ccs/c6748/usblib/Release" -i"C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/binary/c674x/cgt_ccs/grlib/Release" -i"C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/binary/c674x/cgt_ccs/nandlib/Release" -i"C:/ti/pdk_C6748_2_0_0_0/C6748_StarterWare_1_20_03_03/binary/c674x/cgt_ccs/utils/Release" --reread_libs --warn_sections --display_error_number --xml_link_info="edge_video_analytics_linkInfo.xml" --rom_model -o "edge_video_analytics.out" -l"./configPkg/linker.cmd"  "../linker_dsp.cmd" "./wholesceneanalysis.obj" "./vpifapp.obj" "./videosync.obj" "./utils.obj" "./ustdlib.obj" "./uart_local.obj" "./uart_dpr.obj" "./uart_alt.obj" "./tvp5147.obj" "./subsample.obj" "./snapshot.obj" "./serial.obj" "./sensitivity.obj" "./option.obj" "./memory.obj" "./memio.obj" "./main.obj" "./led.obj" "./isl59601.obj" "./i2cgpio.obj" "./hemisphere.obj" "./frame.obj" "./dpr.obj" "./config.obj" "./command.obj" "./codecif.obj" "./clock.obj" "./channel.obj" "./cdce913.obj" "./cbcr422sp_to_rgb565_dsp.obj" "./algozone.obj" "./algovirtualzone.obj" "./algovehicle.obj" "./algotrack.obj" "./algoproc.obj" "./algomain.obj" "./algolntrackdiag.obj" "./algolntrack.obj" "./algolearndiag.obj" "./algolearn.obj" "./algolane.obj" "./algointerface.obj" "./algofog.obj" "./algodet.obj" "./algoconfig.obj" "./algobindata.obj" "./algobike.obj" "./algoUtils.obj" "./adv7343.obj" "./AlgoDayNight.obj" -ldrivers.lib -lgrlib.lib -lplatform.lib -lsystem_config.lib -lusblib.lib -lutils.lib -l"libc.a"

    <Linking>

    'Finished building target: edge_video_analytics.out'

    ' '

    **** Build Finished ****

    .

    Thanks,
    JumpStart

  • That new error is not really an error, but our output parser has a bug and marks that message as an error. As far as I can tell your build finishes without any other issues, so feel free to turn off that flag in Advanced Properties.

  • Hello Sasha,

    It is good to know that there is no build problems.  But I still get the error when I open the app.cfg file and cannot modify the SYS/BIOS setttings (i.e. add new threads, semaphores, change priorities, etc.) because the settings fields are not populated correctly.  What else can I do to identify the error when CCSv5.5 opens up the .cfg file?

    Thanks,
    JumpStart

  • Is there an error message displayed somewhere? What does it say?
    A simple thing you can try is to open your project directory in Windows Explorer and delete the directory .config. But, before you do that, close app.cfg and close CCS. That directory is a temporary one, and will be recreated as soon as you start CCS and open app.cfg.
    If that doesn't help, please post a snapshot of your XGconf window with app.cfg open, and also add the option "-console" to your shortcut for CCS, in the field "target". You should end up with the following content:
    C:\ti\ccsv5\eclipse\ccstudio.exe -console

    After you do that, when you open CCS you'll have one additional console window open. Please post the content of that console window, so I can check if there are any errors there.