This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MPMCL not working with ramfs

Other Parts Discussed in Thread: TCI6636K2H

Hi There,

Greetings !!!


We are using -

Target chip : TCI6636k2h
Target EVM : XTCIEVMK2X   Rev1.1

MCSDK version:
mcsdk_bios_3_00_01_12
mcsdk_linux_3_00_01_12

Note : Code is buiit for c64+


Earlier we were using boot=net for filesystem and using mpmcl utility to download dsp.  (File System -tisdk-rootfs-rt.cpio.gz)
Now we want to use ramfs, and we have done all necessary changes (File System - arago-console-image.cpio.gz).
Our EVM is booting properly but when we try to download dsp using mpmcl, it shows mpmcl as unknown command.
While using nfs, we can see mpm folder in /etc, but same is not there if we use ramfs.

For trial we have tried to use tisdk-rootfs-rt.cpio.gz(size - 33.0 MB) instead of arago-console-image.cpio.gz(7.7 MB) file system with ramfs but it causes kernal panic.

Thanks in advance.

Regards,
Vishal