Hi,
I'm trying to run the image_processing demo (mcsdk_2_01_02_06\demos\image_processing\ipc) on the C6657 EVM it compiles correctly but when I load the master/slave (debug) program they don't get to main() any idea why is that before I start debugging it,
I'm using -
CGT - v7.4.4
XDCtools - 3.25.3.72
IMGLIB - 3.1.1.0
NDK - 2.21.2.43
SYS/BIOS - 6.35.4.50
Thanks,
HR