This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet Interface and IEEE1588, 802.3 AVB

Other Parts Discussed in Thread: AM3874

Do I need to use a specific Ethernet Interface (RGMII, G/MII, RMII) on the AM3874 to support IEEE1588, 802.3?

  • Moving this to the AM387X forum.

  • Don,

    Please refer to the AM387x TRM, chapter 9 3PSW Ethernet Subsystem (EMAC)

    Regards,
    Pavel

  • Pavel,

    I have never used the AM3874 and I have not done an Ethernet hardware design. Chapter 9 is 159 pages long. This answer is not very helpful. I will eventually read the chapter and understand it if this part is selected for the project. Right now I do not have a day to digest it completely. I thought this type of question was what this forum was for.

    Regards,

    Don

  • Hi Don,

    Do you need AVB Rx or Tx? Also what is the end application? PLease let us know..

    Best Regards

    Feroz

  • Don,

    Don Lydon said:
    Do I need to use a specific Ethernet Interface (RGMII, G/MII, RMII) on the AM3874 to support IEEE1588, 802.3?

    This is the feedback from our AVB expert:

    Our MAC ports have hardware support for IEEE1588 (of which the AVB 802.1AS is a subset) and also hardware support for queue management (Rx/Tx) and traffic shaping(Tx-only). In my opinion, the first is probably required for an AVB system, the second is helpful, but not necessarily required. For the rest, it’s all software protocols. There isn’t any requirement to use any particular interface, though on DM814x/AM387x, there is some clocking restrictions when using RGMII because the CPTS clock will be from the same source as the RGMII clock. This means you can’t adjust the CPTS clock for syntonizing to the grand master without potentially causing the 125MHz RGMII clock to go out of spec.

    Regards,
    Pavel

  • Thank you very much Pavel. Your summary was exactly what I needed to understand this complicated part.

    Don

  • The DM814x CPTS only supports layer 2 time-stamping, so you cannot do 1588 in layer 3.

    AudioScience has successfully ported the open source linuxptp to the dm8147 and is using it for 802.1AS in our AVB products.

    steve