This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UIO and PRUSS support with ti-sdk-am335x-evm-06.00.00.00

I have downloaded and now using  the SDK for

LINUXEZSDK-BONE:

Linux EZSDK for BeagleBone, Beaglebone Black

e.g  ti-sdk-am335x-evm-06.00.00.00


There appears to be no support for the uio and pruss. Running Linux on the bbb the /sys/class directory shows that uio is missing. Also, using make menuconfig to modify the kernel .config file, the userspace drivers section is empty and there is no mention of the pruss. So how is  it possible to use this SDK for uio/pruss development.

Regards,