This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI AWB Turning Problem

Hi:

I follow the steps to Tuning AWB,after I sample the raw data, I press the "Tune" button to auto-turn the awb, a dos commad window flashed, i cannot see what error return.
So I open a cmd window and execute the TI_AWB_Tuning.exe in the command console, the error is "Fatal error loading library", some dll files needed is not find.

Firstly, I add matlab dll directory into system environment, restart computer and reexecute TI_AWB_Tuning.exe,the error is also "Fatal error loading library".

Secondly,I tried another way, copy all the dll files which needed to c:/windows/system32 directory, and reexecute it,error changes to:
"C:\Program Files\ImageTunningTool_DM36x\Program\AWB_Tuning>TI_AWB_Tuning.exe
Severe:
MATLAB:I18n:MissingICUData - ICU data not found.
The program '[5416] C:\Program Files\ImageTunningTool_DM36x\Program\AWB_Tuning\T
I_AWB_Tuning.exe: Native' has exited with code 2 (0x2)."

I do not understand the error meaning, so please give some tips,thx
My question is:
1. The way i modify path environment is right or wrong ?
2. If I copy dlls needed to system32 directory, the program can run ok ?
3. If step 2 is ok,what's the last error mean ? Is there any way to solve it.

best regards

lious liu