This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO TRANSACTION FAILED

Hello everyone

When I was using SRIO on C6455 sending data, in the CCS Console it shows a phrase "SRIO TRANSACTION FAILED 3 ".Yes, of course the transmission is failed.  However, I cannot locate this phrase in my source code. Can anyone tell me what is problem? I am wander whether BIOS print it out?

Thank You

XIning

  • Xining,

    If your question is about BIOS, then you should post this question on the BIOS forum and include which version of BIOS you are using, as well as the version information for any SRIO code you are using.

    More likely, the message comes from an SRIO library that you are using. Source should be available for any SRIO drivers delivered by TI. Please search those. If further help is needed, please include more information on any libraries you may be using related to this.

    Regards,
    RandyP

  • Thank You RandyP